The Automation Device Interface (ADI) allows access to specific functions of B&R devices in Windows and Linux. In Windows, the settings of these devices can be read and changed using the Control Center.

  • Features:
  • Changing display-specific parameters
  • Reading out device-specific keys
  • Updating the key configuration
  • Activation of device-specific LEDs on a membrane keypad
  • Reading command devices (e.g. key switches)
  • Reading temperatures, fan speeds and statistical data
  • Reading out operating hours (power-on hours)
  • Reading user settings and factory settings
  • Reading out software versions
  • Updating and backing up the firmware
  • Creating reports about the current system (support assistance)
  • Setting the SDL equalizer value for the SDL cable adjustment
  • Changing the user serial ID

ADI Development Kit

The ADI Development Kit allows B&R Automation Device Interface functions to be accessed from Windows applications created with Microsoft Visual Studio, for example.

  • Features:
  • Header files and import libraries
  • Help files
  • Sample projects
  • ADI DLL: For testing applications if no ADI driver is installed.

ADI .NET SDK

With the ADI .NET SDK, functions of the B&R Automation Device Interface (ADI) can to be accessed from .NET applications created with Microsoft Visual Studio.

  • Features:
  • ADI .NET class library
  • Help files
  • Sample projects
  • ADI DLL: For testing applications if no ADI driver is installed.

Vyberte prosím zemi a jazyk

B&R Logo