Oops, an error occurred! Code: 20260129004919477b069f

Automation Studio Target for Simulink

Automation Studio Target for Simulink offre une interface permettant de générer automatiquement depuis MATLAB/Simulink un code exécutable sur les systèmes cibles B&R. Les outils de simulation et de développement de MATLAB®/Simulink® et d'Automation Studio permettent de passer d'un modèle à un code de qualité en quelques minutes. Les langages C, C++ et texte structuré  IEC 61131-3 sont supportés. Le développement à base de modèles via MATLAB® et Simulink® améliore la qualité de la production et réduit les temps de développement.

Référence produit Description
1TGSIMTS.CRP.00-01 The corporate license allows the use of Automation Studio Target for Simulink by all users at a company at all of a company's sites, including all associated companies, for a period of one year. With the corporate license, it is permitted to license Automation Studio Target for Simulink on a B&R Automation PC that is delivered with the machine if it can be guaranteed that only service personnel working for the machine or plant manufacturer will have access to that instance of Automation Studio. Automation Studio Target for Simulink enables automatic code generation from MATLAB/Simulink for Automation Studio. Support for C, C++ for tasks and function blocks. Simulink external mode, Simulink C-S functions, model referencing and SimScape are also supported. Licensing takes place via activation over the Internet. After one year, the license will automatically be extended an additional year and invoiced accordingly as long as the license has not been canceled before expiration.
1TGSIMTS.SNG.00-01 The single-user license allows exactly one user to use Automation Studio Target for Simulink at any given time for a period of one year. Automation Studio Target for Simulink enables automatic code generation from MATLAB/Simulink for Automation Studio. Support for C, C++ for tasks and function blocks. Simulink external mode, Simulink C-S functions, model referencing and SimScape are also supported. The license is stored on a Technology Guard (dongle). This permits multiple users to share the right to use Automation Studio on different workstations by connecting the Technology Guard with the single-user license to the respective workstation computer. After one year, the license will automatically be extended an additional year and invoiced accordingly as long as the license has not been canceled before expiration. The Technology Guard is not included in the single-user license (separate order required).
1TGSIMTS.SNG.00-02 The single-user license allows exactly one user to use Automation Studio Target for Simulink at any given time for a period of one year. Automation Studio Target for Simulink enables automatic code generation from MATLAB/Simulink for Automation Studio. Support for C, C++ for tasks and function blocks. Simulink external mode, Simulink C-S functions, model referencing and SimScape are also supported. The license is stored in a software license container that is permanently bound to the computer. Transferring the license to another computer is therefore not possible. After one year, the license will automatically be extended an additional year and invoiced accordingly as long as the license has not been canceled before expiration.
1TGSIMTS.STE.00-01 A site license allows the use of Automation Studio Target for Simulink by any number of users at a single company location. The users must be employed at the respective company site but can use Automation Studio Target for Simulink regardless of their location (internationally active service technicians, for example). Automation Studio Target for Simulink enables automatic code generation from MATLAB/Simulink for Automation Studio. Support for C, C++ for tasks and function blocks. Simulink external mode, Simulink C-S functions, model referencing and SimScape are also supported. Licensing takes place via activation over the Internet. After one year, the license will automatically be extended an additional year and invoiced accordingly as long as the license has not been canceled before expiration.

Informations générales

  • Domaines d'application
     
  • Prototypage rapide : implémentation en un clic
  • Conception de programmes de contrôle via l'utilisation de modèles
  • Développement de structures de contrôle complexes
  • Hardware-in-the-loop : émulation de composants système critiques
  • Conception de filtres de valeurs de mesure
  • Analyse de données statistiques
  • Bénéfices :
     
  • Accélération des cycles de développement
  • Productivité accrue
  • Connaissance du process documentée et réutilisable
  • Paramètres de régulation optimisés
  • Bibliothèques de fonction étendues
  • Nombreuses options d'évaluation
  • Utilisation intuitive

Caractéristiques techniques

La génération automatique de code avec B&R Automation Studio Target for Simulink® fait appel aux logiciels suivants :

  • MATLAB® et Simulink® version 2016a ou sup. avec B&R Automation Studio Target for Simulink® version 6.0.0 ou sup.
     
  • Simulink Coder® ou Embedded CoderTM 
     
  • Compilateur C++/C : selon la version de MATLAB®/Simulink® : p. ex. SDK 7.0 ou Visual Studio
     
  • Automation Studio version 3.0.90 ou supérieure pour transférer le code directement à Automation Studio lors de la génération de code.

Echanges de données bidirectionnels

Mode externe 

Le mode externe permet de lier le système cible au modèle Simulink via TCP/IP et de réaliser des échanges de données bidirectionnels de l'un à l'autre pendant l'exécution. Les données peuvent être mises à la disposition du système cible directement depuis le modèle Simulink (via "Scope" ou "Display", par exemple) ou écrites à partir du modèle Simulink sur le système cible (via les blocs Gain ou Constant de Simulink, par exemple).

Veuillez sélectionner un pays et une langue

B&R Logo