Students: Lukas Brünner, Alexander Brader

Supervisors: Anton Deschberger, Albert Schmeitzl

School: HTBLA Braunau am Inn

Project name: WaterStop

Project presentation
Oops, an error occurred! Code: 20260206035619112ac53f
The project concept

The project concept

How did the project come about?

Most houses lack sufficient protection against a burst water pipe and the associated water damage. The reason for this is that the current systems on the market are too expensive and retrofitting is too time-consuming. The two graduates of the HTBLA Braunau am Inn set themselves the task of developing a cost-effective device that can be easily and reliably installed – i.e. retrofitted – into the water circuit of an existing house.

Challenges

Challenges

What is particularly unique, difficult or challenging about your project?

What made the project difficult was, on the one hand, getting a precise measurement of the water flow and creating a water utilization profile. On the other hand, we also had to create a user interface that could be used by an average homeowner. In addition, the data would need to be remotely accessible via a web server.

Solution
Oops, an error occurred! Code: 20260206035619a887877f
Hardware used
Oops, an error occurred! Code: 2026020603561915ca9cc5

Graag land en taal kiezen

B&R Logo